Technical FAQs

Ask a Question

Why is the Animate (Online - Animate) option greyed out when using the Concept Reference Data Editor? This can occur offline or online.

There is an option in the Concept.ini file. The default is for UpdateProjectStateRam to be set to 1. If animate is greyed out when trying
to animate the RDE, make sure this setting is set to 1.

[RDE]
; UpdateProjectStateRam=1 RDE-Synchronize is ON (Default)
; UpdateProjectStateRam=0 RDE-Synchronize is OFF
UpdateProjectStateRam=1


Legacy KB System (APS) Data: RESL213029 V1.0, Originally authored by DaSo on 11/16/2013, Last Edited by DaSo on 11/16/2013
Related ranges: Concept
Was this helpful?
What can we do to improve the information ?