Technical FAQs

Ask a Question

What causes an SKCL.dll error when launching Concept 2.6 on a Win 7 32 bit PC?

Make sure that the version of skcl.dll that is in the C:\windows\system32 folder is version 4.6.0.4 and that the .DLL is registered.


Legacy KB System (APS) Data: RESL213027 V1.0, Originally authored by DaSo on 11/16/2013, Last Edited by DaSo on 11/16/2013
Related ranges: Concept
Was this helpful?
What can we do to improve the information ?