Technical FAQs

Ask a Question

Momentum and Xxmit Error code 120 - 'Could not set PLC UART'

Goals and Symptoms

Xxmit Error code 120 - could not set PLC UART

Causes and Fixes

The most common cause of XMIT / XXMIT error 120 "XXMIT Could Not Set PLC UART" is trying to access a Modbus port that doesn't exist. Since you have a TSX Momentum 171CCC78010 which has 2 Modbus ports, the second most common cause of error 120 "XXMIT Could Not Set PLC UART", it trying to set 2 Stop Bits in a TSX Momentum. The UART that's used for the TSX Momentum Modbus port is not capable of 2 Stop Bits (only 1).


Legacy KB System (APS) Data: RESL213021 V1.0, Originally authored by MiMe on 11/15/2013, Last Edited by MiMe on 11/15/2013
Related ranges: Modbus
Was this helpful?
What can we do to improve the information ?