Technical FAQs

Ask a Question

Does Modbus Plus support Windows XP ?

Goals and Symptoms

Does Modbus Plus support Windows XP ?

Causes and Fixes


Modbus Plus supports Windows XP but only with the new PnP adapters .
Windows XP does not support ISA .
If installing on a desktop computer the PCI-85 ( part numbers 416NHM30030A or 416NHM30032A) adapters must be used .
If installing on a laptop the MB+ PCMCIA (part number 416NHM21234) adapter must be used.


Legacy KB System (APS) Data: RESL212989 V1.0, Originally authored by MiMe on 11/09/2013, Last Edited by MiMe on 11/09/2013
Related ranges: Modbus Plus
Was this helpful?
What can we do to improve the information ?