Technical FAQs

Ask a Question

What is the part number of the cable used for connecting a Magelis XBTGT5330 terminal to a TSX Micro PLC?

The Magelis XBTGT terminal has two ports - COM Port 1 which is of type DB9 and COM PORT 2 which is of type RJ45
1. If using COM PORT 1 (DB9) on Magelis to connect to the TSX Micro

use XBTZ968 + XBTZG909 cable

2. If using COM PORT 2 ( RJ45) on the Magelis to connect to the TSX Micro

use XBTZ9780.


Legacy KB System (APS) Data: RESL212968 V1.0, Originally authored by TVe on 11/08/2013, Last Edited by TVe on 11/08/2013
Related ranges: Magelis XBT GT
Was this helpful?
What can we do to improve the information ?