Technical FAQs

Ask a Question

Can the new 140NRP95400 Fiber Optic Repeater be added into Proworx32 traffic cop?

Goals and Symptoms

Can the new 140NRP95400 Fiber Optic Repeater be added into Proworx32 traffic cop?

Causes and Fixes

No.. 140NRP95400 Fiber Optic Repeater only requires power from the Quantum rack. There is no communication over the back plane between the repeater and the other modules in the rack.


Legacy KB System (APS) Data: RESL212933 V1.0, Originally authored by MiMe on 11/02/2013, Last Edited by MiMe on 11/02/2013
Related ranges: Modbus Plus
Was this helpful?
What can we do to improve the information ?