Technical FAQs

Ask a Question

What is the part number for the memory card used with a Lexium 32x drive?

The part number for the memory card used with a Lexium 32x drive is VW3 M8 705. It can be ordered separately.


Legacy KB System (APS) Data: RESL212924 V1.0, Originally authored by TVe on 11/01/2013, Last Edited by TVe on 11/01/2013
Related ranges: Lexium 32
Was this helpful?
What can we do to improve the information ?