Technical FAQs

Ask a Question

Are the cooling fans on a Lexium 15 drive field replaceable?

The Cooling fans were never sold as a spare part by Schneider. Hence these fans cannot be changed in the field with a Schneider supplied/approved replacement.


Legacy KB System (APS) Data: RESL212923 V1.0, Originally authored by TVe on 11/01/2013, Last Edited by TVe on 11/01/2013
Related ranges: Lexium 15
Was this helpful?
What can we do to improve the information ?