Technical FAQs

Ask a Question

How to run the Stepper drive SD326DU25S2 with 240 V AC input?

The voltage setting is done by using the terminals VS1 and VS2. A jumper needs to be installed between VS1 and VS2 for 115V operation. If the jumper is removed, the drive can be operated with 230 V AC input. This information is referenced in Page 48 of the SD326 user manual.


Legacy KB System (APS) Data: RESL212922 V1.0, Originally authored by TVe on 11/01/2013, Last Edited by TVe on 11/01/2013
Related ranges: SD3
Was this helpful?
What can we do to improve the information ?