Technical FAQs

Ask a Question

Why can't a constant greater then #9999 be entered in the "SU16" instruction using ProWORX 32?


In order to enter a constant greater then #9999 in the "SU16" Math instruction using ProWORX 32, you must have 6 Digit Addressing "On" in "Preferences". Below is a example with "Auto" and then "On" for 6 Digit Addressing in "Preferences":



You will notice that with 5 digit addressing, there's not enough room to put a value greater then #9999.


Legacy KB System (APS) Data: RESL2129 V2.0, Originally authored by MiMa on 09/06/2012, Last Edited by MiOB on 09/06/2012
Related ranges: ProWORX
Was this helpful?
What can we do to improve the information ?