Technical FAQs

Ask a Question

Where is the TM2AMI4LT located in the Advantys software because it is not located under the analog pull down?

The TM2AMI4LT is located under the Thermocouple / RTD pull down of the catalog browser and not under the analog pull down.

Legacy KB System (APS) Data: RESL212893 V1.0, Originally authored by DiSa on 10/28/2013, Last Edited by DiSa on 10/28/2013
Related ranges: Twido
Was this helpful?
What can we do to improve the information ?