Technical FAQs

Ask a Question

What communication protocol is used to flash firmware to the M340 BMX PRA 0100 module?

The Unity Loader is used and firmware can only be flashed to the BMX PRA 00010 module using the Ethernet protocol.


Legacy KB System (APS) Data: RESL212891 V1.0, Originally authored by DaSo on 10/28/2013, Last Edited by DaSo on 10/28/2013
Related ranges: Unity Pro - SoCollaborative software
Was this helpful?
What can we do to improve the information ?