Technical FAQs

Ask a Question

Using Concept FBD and the EN/ENO pins, what effect does the EN pin have on the output?

When the EN pin is TRUE, the block updates the output. When the EN pin is FALSE, the last output is maintained, it does not drop low or go to zero.


Legacy KB System (APS) Data: RESL212862 V1.0, Originally authored by DaSo on 10/24/2013, Last Edited by DaSo on 10/24/2013
Related ranges: Concept
Was this helpful?
What can we do to improve the information ?