Technical FAQs

Ask a Question

On a power cycle of a 171CCC9x030 Momentum M1E CPU, will it load the program from flash memory?

The CPU will load the program from flash memory only if there is no battery backup installed or the threshold voltage level of the battery is low. A battery low status bit can be programmed in logic, if necessary.


Legacy KB System (APS) Data: RESL212856 V1.0, Originally authored by DaSo on 10/24/2013, Last Edited by DaSo on 10/24/2013
Related ranges: Modicon Momentum
Was this helpful?
What can we do to improve the information ?