Technical FAQs

Ask a Question

Are there any Advantys input modules that are sourcing (true low)?

No. All of the Advantys input modules are sink modules.

Legacy KB System (APS) Data: RESL212843 V1.0, Originally authored by DiSa on 10/23/2013, Last Edited by DiSa on 10/23/2013
Related ranges: Modicon STB
Was this helpful?
What can we do to improve the information ?