Technical FAQs

Ask a Question

Is there a procedure on how to perform a program update when using a Quantum Hot Standby System with the 140CHS11000 modules?

Yes, see attachment below:
CHS_PROGRAM_UPDATE.pdfCHS_PROGRAM_UPDATE.pdf


Legacy KB System (APS) Data: RESL212841 V1.0, Originally authored by RoAl on 10/23/2013, Last Edited by RoAl on 10/23/2013
Related ranges: Modicon Quantum
Was this helpful?
What can we do to improve the information ?