Technical FAQs

Ask a Question

Does the M340 PLC maintian state ram during a power cycle?

Yes. By default the values are written to a flash area at power down and then back to state ram at power up.

Was this helpful?
What can we do to improve the information ?