Technical FAQs

Ask a Question

Does the TSX Momentum 171CCC96020 have a TOD (Time of Day) Clock?

No. The TSX Momentum 171CCC96020 does not have a TOD (Time of Day) Clock. If a TOD (Time of Day) Clock is required, you would need to purchase one of the below Option Adapters:
172PNN21022 - ModBus Plus Option Adapter, TOD Clock and Battery Back-up.
172PNN26022 - Redundant ModBus Plus Option Adapter, TOD Clock and Battery Back-up
172JNN21032 - ModBus (RS232/485) Option Adapter, TOD Clock and Battery Back-up.
172JNN21032C - ModBus (RS232/485) Option Adapter, TOD Clock and Battery Back-up, (Conformally Coated).

 
Was this helpful?
What can we do to improve the information ?