Technical FAQs

Ask a Question

What causes the following error during a Unity install? Error 1325 'SchneiderPrivateControlInterface.Interop.dll' is not a valid short file name.

The error, which is shown below, may be the result of a corrupted Unity install. Follow these steps to correct the problem.
1: Remove Unity Pro .

2: Install and run UPcleaner

3: Reinstall Unity Pro

UPCleanerV7final.zipUPCleanerV7final.zip

 

 


Legacy KB System (APS) Data: RESL212801 V1.0, Originally authored by DaSo on 10/18/2013, Last Edited by DaSo on 10/18/2013
Related ranges: Unity Pro - SoCollaborative software
Was this helpful?
What can we do to improve the information ?