Technical FAQs

Ask a Question

What is the maximum tightening torque for the Quantum I/O module terminal strip mounting screws?

The maximum tightening torque for the module terminal strip mounting screws is 10 in-lbs (1.13 Nm).


Legacy KB System (APS) Data: RESL212749 V1.0, Originally authored by RoAl on 10/16/2013, Last Edited by RoAl on 10/16/2013
Related ranges: Modicon Quantum
Was this helpful?
What can we do to improve the information ?