Technical FAQs

Ask a Question

What operating systems are compatible with Vijeo Design'Air?

Vijeo Design'Air is Schneider Electric's application for tablets and smartphones. With Vijeo Design'Air you can use your tablet or smartphone to remotely connect to a Magelis HMI terminal over a wireless network.
It is compatible with the following operating systems:
- Android, version 2.3.3 or later
- iOS version 6 or later.


Legacy KB System (APS) Data: RESL212733 V1.0, Originally authored by DaSo on 10/11/2013, Last Edited by DaSo on 10/11/2013
Related ranges: Vijeo Designer
Was this helpful?
What can we do to improve the information ?