Technical FAQs

Ask a Question

Does the M340 BMXNOExxxx ethernet comm modules support DHCP lease time?

Goals and Symptoms

Does the M340 BMXNOExxxx ethernet comm modules support DHCP lease time?

Causes and Fixes


Yes... As a Server (DHCP Server Supports Timed Leases.. It is a requirement of the DHCP RFC)
No... As a Client ( A client has no way of requesting a specific lease time)

 
 
text

Legacy KB System (APS) Data: RESL212719 V1.0, Originally authored by MiMe on 10/11/2013, Last Edited by MiMe on 10/11/2013
Related ranges: Modicon M340
Was this helpful?
What can we do to improve the information ?