Technical FAQs

Ask a Question

What does the ETHLK LED on the BMXPRA0100 indicate?

The ETHLK is a physical link indicator. It will come on as soon as a valid connection is made between the PRA and an active Ethernet port such as a Hub or Switch. Generally if this is not lit up, it means that either the cable is bad/incorrect or there is no active device (switch is powered down).


Legacy KB System (APS) Data: RESL212707 V1.0, Originally authored by DaSo on 10/09/2013, Last Edited by DaSo on 10/09/2013
Related ranges: Modicon M340
Was this helpful?
What can we do to improve the information ?