Technical FAQs

Ask a Question

What could cause a red I/O fault on the QEIO Drop 140CRA31200 card?

Goals and Symptoms

What could cause a red I/O fault on the QEIO Drop 140CRA31200 card?

Causes and Fixes

There are three reasons why you would get a red I/O fault LED on the 140CRA31200 drop card while getting a solid green LED on (RUN, Mod Status and Net Status):
1) Defective I/O module.. No Active LED (See Note#2 below - External error is detected).
2) I/O Module is missing from Unity project drop I/O map.
3) I/O Modules is in the wrong drop I/O map location.

The LEDs on the front of the adapter module:
140 CRA 312 00:




Legacy KB System (APS) Data: RESL212675 V1.0, Originally authored by MiMe on 10/05/2013, Last Edited by MiMe on 10/05/2013
Related ranges: Modicon Quantum
Was this helpful?
What can we do to improve the information ?