Technical FAQs

Ask a Question

Will the B882-239 High Speed Counter support a quadrature input ?

No, the B882-239 does not support quadrature mode. You would have to use the B883-001 HSC for a quadrature operation.


Legacy KB System (APS) Data: RESL212672 V1.0, Originally authored by DaSo on 10/03/2013, Last Edited by DaSo on 10/03/2013
Related ranges: Modicon 1/2/3/4/5/8/984s
Was this helpful?
What can we do to improve the information ?