Technical FAQs

Ask a Question

Can the Magelis XBTGC have a Profibus card added to it?

 

No. The Magelis XBTGC can not have the Profibus card added. Only the GT and GK series can have the Profibus card added.

Legacy KB System (APS) Data: RESL212669 V1.0, Originally authored by DiSa on 10/03/2013, Last Edited by DiSa on 10/03/2013
Related ranges: Magelis XBT GC
Was this helpful?
What can we do to improve the information ?