Technical FAQs

Ask a Question

How do you order a BSH Motor with IP67 protection class rating?

Goals and Symptoms

This resolution explains how to order a BSH motor with IP67 protection class rating.

Causes and Fixes

To achieve IP67 protection class rating, the corresponding IP67 kit has to be mounted on the respective BSH motor. Degree
of protection IP65 is a pre-requisite for the use of the IP67 kit. The IP67 kit is used to connect compressed air to the motor.
The compressed air generates a permanent over-pressure inside the motor. This over-pressure inside the motor is used to obtain IP67 degree of protection.

The following table lists the IP67 kits offered for the different BSH motors.


Legacy KB System (APS) Data: RESL212657 V1.0, Originally authored by TVe on 10/02/2013, Last Edited by TVe on 10/02/2013
Related ranges: Other Motion controllers
Was this helpful?
What can we do to improve the information ?