Technical FAQs

Ask a Question

When wiring a BMXDAO1605 discrete output module, is the 120VAC power to each group of the module a line or neutral connection ?

Each group of the BMXDAO1605 module, should have a fused 120 VAC line connection to the module. The 120VAC neutral is connected to each field device.


Legacy KB System (APS) Data: RESL212608 V1.0, Originally authored by DaSo on 09/26/2013, Last Edited by DaSo on 09/26/2013
Related ranges: Modicon M340
Was this helpful?
What can we do to improve the information ?