Technical FAQs

Ask a Question

Using ProWORX or Modsoft, how can I scale my Momentum 0-4095 PID2 Mv (Output) value to a 0-32000 INT with the result in a single register?

See attached resolution.
Scaling 0-4095 to 0-32000.pdf

Was this helpful?
What can we do to improve the information ?