Technical FAQs

Ask a Question

Disabling a section in Concept.

To disable as section in Concept :
Launch the Reference Data Editor by pressing Ctrl R. Double click on a number in the left column. Choose a blank line.
This will bring up the Lookup Variables window.
Choose Datatype: Structured.
Highlight the name of the section you wish to disable.
Click on <Components> in the lower left corner.
Choose disable: BOOL. <OK>.
This creates a variable called SECTIONNAME:disable.
Set this variable to 1 to disable the section and to 0 to enable the section.


Legacy KB System (APS) Data: RESL212564 V1.0, Originally authored by DaSo on 09/23/2013, Last Edited by DaSo on 09/23/2013
Related ranges: Concept
Was this helpful?
What can we do to improve the information ?