Technical FAQs

Ask a Question

How can Unity Pro error "The thread is not assigned to any session. <err-0001-0168> Attempt to use sessions before Objectstore has been initialized. (err_no_session)" be corrected?

This error usually occurs when launching Unity Pro. The working drive specified in the registry may be incorrect.
Open the Registry Editor and go to the following path:

HKEY_CURRENT_USER\SchneiderElectric\Unity ProXL\ProductVersion\Options\UnityXL
Make sure the working drive is a valid drive, usually C:\.


Legacy KB System (APS) Data: RESL212560 V1.0, Originally authored by DaSo on 09/21/2013, Last Edited by DaSo on 09/21/2013
Related ranges: Unity Pro - SoCollaborative software
Was this helpful?
What can we do to improve the information ?