Technical FAQs

Ask a Question

What accessories are needed with ILA2TxxxPC1Ax type Lexium Integrated Drive?

The ILA2TxxxPC1Ax type motor will come equipped with industrial connectors on the motor.
Therefore you must order the appropriate power cable and field-bus connectors as accessories because these do not come supplied with the motor.

The part number for the Modbus TCP connector set is VW3L5T000.

The Power cable is available in various lengths and the part numbers are as follows.

VW3L30001R30 = 3 meter long
VW3L30001R50 = 5 meter long
VW3L30001R100 = 10 meter long
VW3L30001R150 = 15 meter long
VW3L30001R200 = 20 meter long


Legacy KB System (APS) Data: RESL212548 V1.0, Originally authored by TVe on 09/20/2013, Last Edited by TVe on 09/20/2013
Related ranges: Lexium ILA, ILE, ILS
Was this helpful?
What can we do to improve the information ?