Technical FAQs

Ask a Question

Advantys Configuration software version 7.0 and configuration of the ATV32 using the Canbus Extension Module

Goals and Symptoms

To configure the ATV32 as a CANopen device when using the Advantys STB CANopen extension module.

Facts and Changes

Advantys Configuration software version 7.0

Causes and Fixes

There is a patch that has to be loaded to add the ATV32 to the catalog to be able to configure the module as a device on the CANopen extension module network. Below is the patch and update User Manual.

Attachments

(Removed File URL: 212523_DF0A/patch_advantys_v7_0_0_3.zip)(Removed Image URL: /PubResEXPORT.nsf/2b87ee90be777fc085257c28006ee4ef/640e1373e24c387bc1257bc300118c60/fl_block_5/0.EA?OpenElement&FieldElemFormat=gif)(Removed File URL: 212523_DF0A/STB_CANopen_std_devices_7_2013.zip)(Removed Image URL: /PubResEXPORT.nsf/2b87ee90be777fc085257c28006ee4ef/640e1373e24c387bc1257bc300118c60/fl_block_5/0.7A6?OpenElement&FieldElemFormat=gif)


Legacy KB System (APS) Data: RESL212523 V1.0, Originally authored by DaSo on 09/18/2013, Last Edited by DaSo on 09/18/2013
Related ranges: Modicon STB
Was this helpful?
What can we do to improve the information ?