Technical FAQs

Ask a Question

Do I need to match the marked PV, RL and SV versions for the Unity Pro 140CPU67xxx PLCs in a Hot Standby configuration?

No, but the actual Firmware and CoPro versions that are in the CPU do need to match. The PV (Product Version) and RL (Release) can be different. The SV ( Software Version) is indicative of the firmware version that was shipped in the PLC from the factory. If the SV markings do not match, you need to ensure that the loaded firmware/copro is the same.


Legacy KB System (APS) Data: RESL212514 V1.0, Originally authored by DaSo on 09/17/2013, Last Edited by DaSo on 09/17/2013
Related ranges: Modicon Quantum
Was this helpful?
What can we do to improve the information ?