Technical FAQs

Ask a Question

Terminal numbers 13,14, 27 and 28 are not assigned on the BMXAMI0810. Can these terminals be used as a marshalling point for field wiring?

These pins are not connected internally. You can use terminal numbers 13, 14, 27 & 28 as a marshalling point for field wiring. 


Legacy KB System (APS) Data: RESL212509 V1.0, Originally authored by RoAl on 09/17/2013, Last Edited by RoAl on 09/17/2013
Related ranges: Modicon M340
Was this helpful?
What can we do to improve the information ?