Technical FAQs

Ask a Question

Can I change Twido IO modules to a different type of module without changing the configuration?

Some IO modules can be changed if they are discrete modules with the same IO count. e.g. TM2DDO8TT and TM2DDO8UT can be exchanged and juts wired differently (sink -vs- source. Other than that you can not change a 8 point card with a 16 point card without changing it in the configuration and downloading it to the controller.

Legacy KB System (APS) Data: RESL212508 V1.0, Originally authored by DiSa on 09/17/2013, Last Edited by DiSa on 09/17/2013
Related ranges: Twido
Was this helpful?
What can we do to improve the information ?