Technical FAQs

Ask a Question

Is there an EFB in Unity which will swap the high and low bytes within a String?

Yes, the STRING_TO_ASCII_INV EFB will swap the high and low bytes within an ASCII string.


Legacy KB System (APS) Data: RESL212484 V1.0, Originally authored by DaSo on 09/12/2013, Last Edited by DaSo on 09/12/2013
Related ranges: Unity Pro - SoCollaborative software
Was this helpful?
What can we do to improve the information ?