Technical FAQs

Ask a Question

Does the TSXETG100 support ASCII communication?

The TSXETG100 gateway only supports the Modbus\RTU or Modbus\ASCII serial communication protocols. It does not support 7-bit or 8-bit ASCII character mode communication.


Was this helpful?
What can we do to improve the information ?