Technical FAQs

Ask a Question

Using Concept, can the TSX Momentum PLC read 0X references direct from a Modbus TCP Ethernet device using IO Scanner or standard instructions?

No. Concept IO scanner and the built-in Modbus TCP communication blocks will only read and write to 4X registers.

 
Was this helpful?
What can we do to improve the information ?