Technical FAQs

Ask a Question

Can I use an M340 harsh environment module in an M340 configuration that only has standard modules?

Yes. A harsh environment module is mapped and wired in the same way as a standard module and could be used as a replacement.

Was this helpful?
What can we do to improve the information ?