Technical FAQs

Ask a Question

Is there a health status bit for the Quantum 140XBE10000 backplane extender module?

 

 
No. The Quantum 140XBE10000 backplane extender module does not have a personality chip like I/O modules so there's no health bit information available.
This module simply extends the bus of the Primary backplane to the bus of the Secondary backplane.

Legacy KB System (APS) Data: RESL212388 V1.0, Originally authored by DiSa on 08/28/2013, Last Edited by DiSa on 08/28/2013
Related ranges: Modicon Quantum
Was this helpful?
What can we do to improve the information ?