Technical FAQs

Ask a Question

Why will my Concept project convert on one of my Unity Pro v7.0 installs, but on a second it gives me a "Bad XEF/ZEF file format" error?

With Unity Pro V7.0 everything needed for the conversion should have installed automatically. It is possible that one of the installation files has become corrupted. Run the Install DVD again and select 'Repair'.

Was this helpful?
What can we do to improve the information ?