Technical FAQs

Ask a Question

What is the part number for the EMC grounding hardware used with Lexium 05, Lexium SD328 and Lexium SD326 ?

The ordering number for the EMC kit for Lexium SD32x and Lexium05 is VW3M2101
This is a complete set of all the original hardware needed to ground the and clamp the cabling to the drive.

VW3M2101 = EMC KIT SIZE-1

This kit consists of all the hardware that originally came equipped with the drive and can be ordered in the event the hardware has been lost or damaged.


Legacy KB System (APS) Data: RESL212361 V1.0, Originally authored by TVe on 08/24/2013, Last Edited by TVe on 08/24/2013
Related ranges: Lexium 05, Lexium SD3
Was this helpful?
What can we do to improve the information ?