Technical FAQs

Ask a Question

What are the cable part numbers for M340 IO modules with 40 pin connections ?

The following M340 IO modules require preconfigured 40 pin connector cable with color coded flying leads.
Table below shows module and cable part numbers.

 
Discrete Module Connection Cable Part # Qty needed
BMX DDI 3202 1 x 40 BMX FCW 303, 503, 1003 ( 1 )
BMX DDI 6402 2 x 40 BMX FCW 303, 503, 1003 ( 2 )
BMX DDM 3202 1 x 40 BMX FCW 303, 503, 1003 ( 1 )
BMX DDO 3202 1 x 40 BMX FCW 303, 503, 1003 ( 1 )
BMX DDO 6402 2 x 40 BMX FCW 303, 503, 1003 ( 2 )
text text
AnalogModule text
BMX ART 0414 1 x 40 BMX FCW 301S*, 501S* ( 1 )
BMX ART 0814 2 x 40 BMX FCW 301S*, 501S* ( 2 )
* S suffix denotes shielded cable for Analog IO.

Legacy KB System (APS) Data: RESL212360 V1.0, Originally authored by DiSa on 08/24/2013, Last Edited by DiSa on 08/24/2013
Related ranges: Modicon M340
Was this helpful?
What can we do to improve the information ?