Technical FAQs

Ask a Question

With Unity Pro, I need to modify the settings of my NOE card but I can not alter the Ethernet_1 settings. Why are they grayed out?

If an ethernet port has the Ethernet_1 configuration linked to it, the settings will be grayed out. Double click on the Ethernet port of the NOE card in the local bus and select 'No Link'. You will now be able to edit the settings before you re-link it.


Legacy KB System (APS) Data: RESL212358 V1.0, Originally authored by DaSo on 08/24/2013, Last Edited by DaSo on 08/24/2013
Related ranges: Unity Pro - SoCollaborative software
Was this helpful?
What can we do to improve the information ?