Technical FAQs

Ask a Question

Using ProWORX NxT, what would cause a miscompare for holding register contents on a project that I just loaded to the PLC?

This typically means that the PLC is or has been in Run mode and the holding register contents have changed. This is normal operation.

Was this helpful?
What can we do to improve the information ?