Technical FAQs

Ask a Question

Does the Momentum PLC I/O Scanner support Device Control when configured with ProWORX or Concept programming software?

No. The Device Control Block function is not supported when configuring I/O Scanner within the Momentum PLC family with Concept or ProWORX.


Legacy KB System (APS) Data: RESL212356 V1.0, Originally authored by DaSo on 08/24/2013, Last Edited by DaSo on 08/24/2013
Related ranges: Modicon Momentum
Was this helpful?
What can we do to improve the information ?