Technical FAQs

Ask a Question

TSXETG100 Dip Switch Settings for RS485 Biasing and Termination.

Goals and Symptoms

TSXETG100 Dip Switch Settings for RS485 Biasing and Termination.

Causes and Fixes

TSXETG100 Dip Switch Settings for RS485 Biasing and Termination.
The following DIP switch settings are recommended for 4-wire and 2-wire daisy
chains.

 


Legacy KB System (APS) Data: RESL212355 V1.0, Originally authored by MiMe on 08/24/2013, Last Edited by MiMe on 08/24/2013
Related ranges: ConneXium - Ethernet
Was this helpful?
What can we do to improve the information ?