Technical FAQs

Ask a Question

What causes a 'card adapter full' error when editing online using Unity Pro?

After online editing a memory reorganization is sometimes needed. Go to PLC - Memory Consumption - and check the Fragmentation.
If it exceeds 5%, we recommend performing a <Pack> command. This can be done offline or online, with the PLC running or stopped.


Legacy KB System (APS) Data: RESL212349 V1.0, Originally authored by DaSo on 08/23/2013, Last Edited by DaSo on 08/23/2013
Related ranges: Unity Pro - SoCollaborative software
Was this helpful?
What can we do to improve the information ?