Technical FAQs

Ask a Question

How can I add located variables to FBD pins by selecting addresses but have them display as variable names in logic.

Double click on the pin and then left click on the ellipsis. With the cursor on one of the variables in the list, right click and select 'customize columns'. Place a check mark on 'Address' and move it up in location (click on the blue box with arrow) so that it is directly under 'Name' and hit 'OK'. Now you will see the addresses to the right of the variable names. If desired, you can sort by address by clicking on the word 'Address' in the menu.


Legacy KB System (APS) Data: RESL212331 V1.0, Originally authored by DaSo on 08/20/2013, Last Edited by DaSo on 08/20/2013
Related ranges: Unity Pro - SoCollaborative software
Was this helpful?
What can we do to improve the information ?